M12 Push-Pull: The Universal Quick-Connect System | Murrelektronik

27. novembre 2018

M12 Push-Pull: The Universal Quick-Connect System

Anyone who spends a lot of time installing M12 cordsets must have asked themselves if a reliable and universal quick-connection system exists that is capable of coping with the full spectrum of stresses and strains. In future, the answer to that will be “Yes!”

M12 Push-Pull - cordsets

The M12 Push-Pull is a standard system that enables M12 cordsets to be connected in record time. Leading connector manufacturers have worked together to deliver a top-quality and standardized product to the market.

It connects by using a push-pull system. The technician can hook up the connector very quickly and without tools since each wire has an identical connector pattern. This is unlike the conventional M12 because using the M12 Push-Pull reduces the installation time by about 80 percent. This is extremely efficient in installations where space is limited – the male connectors with push-pull connection technology offer several benefits.

Is there a risk of achieving speed at the expense of process safety? Clear answer: no! With the M12 Push-Pull system, male and female connectors lock into an accurately aligned contour, and once connected and locked in, each connection is leak-proof and is IP67 protected. Acoustic and tactile feedback provide the technician with the feedback that the cordset is correctly connected.

Our forecast: The new standard M12 Push-Pull will be the trigger to the rising trend of M12 connectors, making it the first choice for many other applications! The success story of the M12 Push-Pull cordset has just begun.

   

Scarica

Novità da Murrelektronik

Achieve More Together - Murrelektronik becomes 60th member of Single Pair Ethernet System Alliance

Networking is the main topic of the Industrial Internet of Things (IIoT). The technology behind Single Pair Ethernet has the potential to drive this topic forward. Murrelektronik…

Altro

Murrelektronik Austria moves into new office space at Vienna Airport

A new chapter has begun for automation technology specialist Murrelektronik in Austria as it takes up residence at its new address: “Office Park 4” at Vienna AirportCity. The…

Altro

Martin Kram becomes Vice President Sales Germany at Murrelektronik

Murrelektronik, a specialist in decentralized automation technology for machines and plants, is making a mid-year change to its sales management team. Martin Kram has been Vice…

Altro

Benvenuto/a
Newsletter
Siamo qui per te!
Sempre pronti a rispondere alle tue domande...