Murrelektronik is looking forward to the possiblities with Single Pair Ethernet | Murrelektronik

20. febbraio 2020

SPE is very important to us

Murrelektronik is looking forward to the possiblities with Single Pair Ethernet (SPE). As a connection specialist for the electrical installation of machines and systems, Murrelektronik is a powerful partner within a strong network.

This network is driving the technology forward with determination and with a view to future challenges in automation. Jürgen Zeltwanger, Managing Director at Murrelektronik, is convinced of the development: "With SPE, we achieve integrated communication on the basis of Ethernet - from the cloud or the controller via switches to the sensors and actuators. As a connection specialist, this is naturally close to our heart".

Murrelektronik sees the trend that SPE has the potential to become the physical platform for state-of-the-art installation concepts with today's Ethernet-based fieldbus protocols such as PROFINET, Ethernet/IP (and the futures such as OPC UA TSN-FLC).  The focus is on the clearly visible cost-benefit factor.

Murrelektronik believes that the two-wire connection via Single Pair Ethernet offers decisive advantages. "The electronic connection in machines and systems is becoming more economical and efficient. By embedding SPE technology in the relevant world of standards and the simultaneous transmission of power and data, this technology has the potential to become the backbone of the Industrial Internet of Things in the future," explains Jürgen Zeltwanger.

Scarica

Novità da Murrelektronik

Cube67 Diagnostics Gateway: Diagnostics Made Easy

Murrelektronik's Cube fieldbus system offers extensive diagnostic options. A new diagnostics gateway makes access to this data even easier. This solution is easy to implement,...

Altro

Efficient and Cost-Effective Installation Concepts

Schmid Maschinenbau is a powerful partner of the automotive industry. The company's custom machines and production lines are used by numerous well-known automotive manufacturers...

Altro

A Perfect System to Monitor Current

Mico Pro is Murrelektronik's innovative 24 VDC current monitoring system. The modular design makes it possible to create systems that fit the application perfectly – which adds...

Altro

Questo sito utilizza i cookie per assicurarti una migliore esperienza di navigazione. Continuando a navigare, accetti l'uso di questi cookie. Per maggiori informazioni.

Benvenuto/a
Siamo qui per te!
Sempre pronti a rispondere alle tue domande...